HomeDownloadSponsorMotivesVisionOverview | ReferencesFeedbackAbout

  Content overview
 

The total package that is available here today for free contains professional educational material corresponding to 240 typed pages. It contains about 200 illustrations and photos.

Environmental Education

The “Basic Course” suits everybody no matter what level of understanding you are on. The course should take about one day of studies to go through. There is a separate glossary and also “study questions” after each chapter to measure your understanding of the material.

The Advanced Course (available in Swedish and Japanese) is found adjacent to the Basic Course and contains tools for organisations to put to use in their environmental work. The Advanced Course contains for example ISO, EMAS, ecological footprints, Factor 4 and 10 and much more.

There is also an environmental test that anyone can do to test if they are environmental friendly or not. This is also available in Swedish and Japanese. This test is designed to take about 15 minutes to go thorough as long as you do not engage yourself in the “in depth material”.

Have fun!

Miljöutbildarna HB - Louise Wersäll, VD | Ibsengatan 40
168 47 Bromma | louise@milou.se.com | Mobile 0046739376066